Solid Edge Framework Type Library
AddMaterialToLibrary Method
Description
Syntax
Visual Basic
Public Sub AddMaterialToLibrary( _
   ByVal bstrMatName As String, _
   ByVal bstrLibrary As String, _
   ByVal bstrMaterialPath As String, _
   ByVal lNumProps As Long, _
   ByVal varPropList As Variant, _
   ByVal bstrFaceStyle As String, _
   ByVal bstrFillStyle As String _
) 
Parameters
bstrMatName
bstrLibrary
bstrMaterialPath
lNumProps
varPropList
bstrFaceStyle
bstrFillStyle
Example
Imports System
Imports System.Runtime.InteropServices

Namespace Examples
    Friend Class Program
        <STAThread>
        Shared Sub Main(ByVal args() As String)
            Dim application As SolidEdgeFramework.Application = Nothing
            Dim partDocument As SolidEdgePart.PartDocument = Nothing
            Dim materialTable As SolidEdgeFramework.MatTable = Nothing

            Try
                ' See "Handling 'Application is Busy' and 'Call was Rejected By Callee' errors" topic.
                OleMessageFilter.Register()

                ' Attempt to connect to a running instance of Solid Edge.
                application = DirectCast(Marshal.GetActiveObject("SolidEdge.Application"), SolidEdgeFramework.Application)
                partDocument = CType(application.ActiveDocument, SolidEdgePart.PartDocument)
                materialTable = application.GetMaterialTable()
                materialTable.SetActiveDocument(partDocument)

                Dim materialName = "MyMaterial"
                Dim libraryName = "Materials"
                Dim materialsPath = "Others"
                Dim faceStyle = "Copper"
                Dim fillStyle = "ANSI33(Brass)"
                ' Define exactly 9 material properties in this specific order (pay attention to the units!!):
                ' 1) Density [kg/m3]
                ' 2) Coef. of Thermal Exp. [1/ºC]
                ' 3) Thermal Conductivity [W/mºC]
                ' 4) Specific Heat [J/kgºC]
                ' 5) Modulus of Elasticity [Pa]
                ' 6) Poisson's Ratio[unitless]
                ' 7) Yield Stress [Pa]
                ' 8) Ultimate Stress [Pa]
                ' 9) Elongation % [unitless]
                Dim propList = New Object() { 7888.0, 0.0, 51.0, 500.0, 69985996255.0, 711.0, 250000000.0, 745000000.0, 0.0 }

                materialTable.AddMaterialToLibrary(materialName, libraryName, materialsPath, propList.Length, propList, faceStyle, fillStyle)

                materialTable.DeleteMaterialFromLibrary(materialName, libraryName)
            Catch ex As System.Exception
                Console.WriteLine(ex)
            Finally
                OleMessageFilter.Unregister()
            End Try
        End Sub
    End Class
End Namespace
using System;
using System.Runtime.InteropServices;

namespace Examples
{
    class Program
    {
        [STAThread]
        static void Main(string[] args)
        {
            SolidEdgeFramework.Application application = null;
            SolidEdgePart.PartDocument partDocument = null;
            SolidEdgeFramework.MatTable materialTable = null;

            try
            {
                // See "Handling 'Application is Busy' and 'Call was Rejected By Callee' errors" topic.
                OleMessageFilter.Register();

                // Attempt to connect to a running instance of Solid Edge.
                application = (SolidEdgeFramework.Application)Marshal.GetActiveObject("SolidEdge.Application");
                partDocument = (SolidEdgePart.PartDocument)application.ActiveDocument;
                materialTable = application.GetMaterialTable();
                materialTable.SetActiveDocument(partDocument);

                var materialName = "MyMaterial";
                var libraryName = "Materials";
                var materialsPath = "Others";
                var faceStyle = "Copper";
                var fillStyle = "ANSI33(Brass)";
                // Define exactly 9 material properties in this specific order (pay attention to the units!!):
                // 1) Density [kg/m3]
                // 2) Coef. of Thermal Exp. [1/ºC]
                // 3) Thermal Conductivity [W/mºC]
                // 4) Specific Heat [J/kgºC]
                // 5) Modulus of Elasticity [Pa]
                // 6) Poisson's Ratio[unitless]
                // 7) Yield Stress [Pa]
                // 8) Ultimate Stress [Pa]
                // 9) Elongation % [unitless]
                var propList = new object[] { 7888.0, 0.0, 51.0, 500.0, 69985996255.0, 711.0, 250000000.0, 745000000.0, 0.0 };

                materialTable.AddMaterialToLibrary(materialName, libraryName, materialsPath, propList.Length, propList, faceStyle, fillStyle);

                materialTable.DeleteMaterialFromLibrary(materialName, libraryName);
            }
            catch (System.Exception ex)
            {
                Console.WriteLine(ex);
            }
            finally
            {
                OleMessageFilter.Unregister();
            }
        }
    }
}
See Also

MatTable Object  | MatTable Members