Solid Edge Framework Type Library : MatTable Object |
AddCustomProperty | Adds the custom property for input material. |
AddMaterial | Adds material to material library. |
AddMaterialToFavorites | Adds the input material to the list of favorite materials. |
AddMaterialToLibrary | |
ApplyGageFromGageTableToDoc | Apply Gage to a document from Gage table excel. |
ApplyGageFromLibraryToDoc | Apply Gage to a document from input library. |
ApplyMaterial | This API is used to apply specific material for a document. |
ApplyMaterialToDoc | This method will apply material from given library to the document. |
ApplyMaterialToFile | Apply Material to the File |
ClearMRUList | Clears the current MRU list. |
CreateNewDirectory | Creates an empty directory at specified level in the library |
CreateNewMaterialLibrary | This API will create a new material library. |
DeleteCustomProperty | Deletes the custom property of a material. |
DeleteDirectory | |
DeleteMaterial | Deletes material from library. |
DeleteMaterialFromLibrary | Deletes input material from specified library. |
EditOpenGageExcelFile | This method is used to open the Gage file for editing. |
ExportMaterialDataToFile | Writes out all the material data of input material library into XML or EXCEL file. |
GetCountOfCustomProperties | Returns the count of custom properties of a material from specified library. |
GetCurrentGageName | This method is used to fetch the name of currently applied gage of a sheet metal document. |
GetCurrentMaterialName | This method is used to fetch the name of currently applied material of a sheet metal document. |
GetCustomMaterialPropertyFromDoc | This method will return custom property for input material from specified document. |
GetCustomMaterialPropertyFromLibrary | This method will return custom property for input material from specified library. |
GetDefaultGageFileName | This method is used to get the complete path of the gage excel file. |
GetFavoriteMaterialList | Returns the list of favorite materials and their corresponding libraries. |
GetMaterialLibraryFileList | Returns the list containing full path of material libraries in materials folder. |
GetMaterialLibraryList | Returns the list containing only names of material libraries in materials folder. |
GetMaterialList | Returns material list from library. |
GetMaterialListFromLibrary | This API will return the list of materials from a specific library. The library can be full path or only name of the library file. |
GetMaterialPropValueFromDoc | Return Material's property from input document. |
GetMaterialPropValueFromLibrary | Returns the property value of a material from specified library. |
GetMaterialsFolderPath | Returns the material library folder path. |
GetMatLibFileName | Returns material library name. |
GetMatPropValue | Returns material property value. |
GetMRUMaterialLimit | Returns the current limit of MRU materials. |
GetMRUMaterialList | Returns the list of most recently used materials and their corresponding libraries. |
GetNeutralFactor | Get Neutral factor value from excel |
GetOODStatusofMaterialAndGage | Checks Out of Date Material and Gage properties in the Material Table |
GetPSMGaugeInfoForDoc | This API is used to get all the gage related information from a sheet metal document. |
GetPSMGaugeListFromExcel | This method is used to obtain list of Gages from a Gage table. |
ImportMaterialDataFromFile | Overwrites all the data of input material library with data from XML or EXCEL file. |
PerformGageDataValidation | This method is used to validate a Gage for data integrity. |
RenameDirectory | Renames existing directory with new name. |
RenameLibrary | Renames existing library with new name. |
RenameMaterial | Renames the input material with new name. |
SetActiveDocument | |
SetDocumentToGageTableAssociation | This method will create an association between the sheet metal file and the Gage table. |
SetMaterialPropValueToLibrary | Sets the value for property of a material from specified library. |
SetMaterialsFolderPath | |
SetMaterialToGageTableAssociation | This method is used to create an association between a material and a Gage table. |
SetMatPropValue | Sets material property value. |
SetMRUMaterialLimit | Sets the limit value for MRU materials. |
UpdateOODMaterialAndGageProperties | Update Out of Date Material and Gage properties in the Material Table |
UseNeutralFactorFromExcel | This method is used to decide source of the Neutral Factor. |
WriteMaterialDataToXML | Writes material table data to XML file. |
WriteMatLibFileFromXML |