Solid Edge Part Type Library
ToggleRefPlanesDisplay Method
If True, the reference planes are displayed. If False, the reference planes are not displayed.
Description
Controls the display of the reference planes.
Syntax
Visual Basic
Public Sub ToggleRefPlanesDisplay( _
   ByVal Display As Boolean _
) 
Parameters
Display
If True, the reference planes are displayed. If False, the reference planes are not displayed.
See Also

WeldmentDocument Object  | WeldmentDocument Members