Solid Edge Part Type Library
SaveAsJT Method
Description
Saves the referenced document to JT format with specified options.
Syntax
Visual Basic
Public Sub SaveAsJT( _
   ByVal NewName As String, _
   Optional ByVal Include_PreciseGeom As Variant, _
   Optional ByVal Prod_Structure_Option As Variant, _
   Optional ByVal Export_PMI As Variant, _
   Optional ByVal Export_CoordinateSystem As Variant, _
   Optional ByVal Export_3DBodies As Variant, _
   Optional ByVal NumberofLODs As Variant, _
   Optional ByVal JTFileUnit As Variant, _
   Optional ByVal Write_Which_Files As Variant, _
   Optional ByVal Use_Simplified_TopAsm As Variant, _
   Optional ByVal Use_Simplified_SubAsm As Variant, _
   Optional ByVal Use_Simplified_Part As Variant, _
   Optional ByVal EnableDefaultOutputPath As Variant, _
   Optional ByVal IncludeSEProperties As Variant, _
   Optional ByVal Export_VisiblePartsOnly As Variant, _
   Optional ByVal Export_VisibleConstructionsOnly As Variant, _
   Optional ByVal RemoveUnsafeCharacters As Variant, _
   Optional ByVal ExportSEPartFileAsSingleJTFile As Variant _
) 
Parameters
NewName
Include_PreciseGeom
Prod_Structure_Option
Export_PMI
Export_CoordinateSystem
Export_3DBodies
NumberofLODs
JTFileUnit
Write_Which_Files
Use_Simplified_TopAsm
Use_Simplified_SubAsm
Use_Simplified_Part
EnableDefaultOutputPath
IncludeSEProperties
Export_VisiblePartsOnly
Export_VisibleConstructionsOnly
RemoveUnsafeCharacters
ExportSEPartFileAsSingleJTFile
See Also

WeldmentDocument Object  | WeldmentDocument Members  | Solid Edge ST3 - What's New