Solid Edge Part Type Library
SaveAs Method
Specifies the name of the saved file. The other optional parameters are not currently supported.
Not currently supported. However, to save a file as a template, you can save it under the template directory.
When saving as PDF, a value of True saves a 3D PDF where a value of False saves a 2D PDF.  This argument is unsupported for other file types.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Description
Saves the referenced document to a new name, directory, or format.
Syntax
Visual Basic
Public Sub SaveAs( _
   ByVal NewName As String, _
   Optional ByVal IsATemplate As Variant, _
   Optional ByVal FileFormat As Variant, _
   Optional ByVal ReadOnlyEnforced As Variant, _
   Optional ByVal ReadOnlyRecommended As Variant, _
   Optional ByVal NewStatus As Variant, _
   Optional ByVal CreateBackup As Variant, _
   Optional ByVal UpdateLinkInContainer As Variant, _
   Optional ByVal UpdateAllLinksInContainer As Variant _
) 
Parameters
NewName
Specifies the name of the saved file. The other optional parameters are not currently supported.
IsATemplate
Not currently supported. However, to save a file as a template, you can save it under the template directory.
FileFormat
When saving as PDF, a value of True saves a 3D PDF where a value of False saves a 2D PDF.  This argument is unsupported for other file types.
ReadOnlyEnforced
Not currently supported.
ReadOnlyRecommended
Not currently supported.
NewStatus
Not currently supported.
CreateBackup
Not currently supported.
UpdateLinkInContainer
Not currently supported.
UpdateAllLinksInContainer
Not currently supported.
Remarks
When used to copy a source document to a new file name, SaveAs assigns property set values to the new document to give the document a unique identity, changes the name of the document, and updates the window titles and most recently used menu items.
See Also

WeldmentDocument Object  | WeldmentDocument Members