Solid Edge Part Type Library
GetUserPhysicalProperties Method
Returns the volume.
Returns the surface area.
Returns the mass.
Returns the x-, y-, and z-coordinates of the center of gravity.
Returns the x-, y-, and z-coordinates of the center of volume, made with respect to the global origin.
Returns the lxx, lyy, lzz, lxy, lxz, and lyz components of the global moments of inertia.
Returns the lxx, lyy, and lzz components of the principal moments of inertia.
Returns the orientation of the principal axes.
Returns three values that specify the radii of gyration.
Description
Method to get the user defined physical properties
Syntax
Visual Basic
Public Sub GetUserPhysicalProperties( _
   ByRef Volume As Double, _
   ByRef Area As Double, _
   ByRef Mass As Double, _
   ByRef CenterOfGravity() As Double, _
   ByRef CenterOfVolume() As Double, _
   ByRef GlobalMomentsOfInertia() As Double, _
   ByRef PrincipalMomentsOfInertia() As Double, _
   ByRef PrincipalAxes() As Double, _
   ByRef RadiiOfGyration() As Double _
) 
Parameters
Volume
Returns the volume.
Area
Returns the surface area.
Mass
Returns the mass.
CenterOfGravity
Returns the x-, y-, and z-coordinates of the center of gravity.
CenterOfVolume
Returns the x-, y-, and z-coordinates of the center of volume, made with respect to the global origin.
GlobalMomentsOfInertia
Returns the lxx, lyy, lzz, lxy, lxz, and lyz components of the global moments of inertia.
PrincipalMomentsOfInertia
Returns the lxx, lyy, and lzz components of the principal moments of inertia.
PrincipalAxes
Returns the orientation of the principal axes.
RadiiOfGyration
Returns three values that specify the radii of gyration.
See Also

WeldmentDocument Object  | WeldmentDocument Members