Solid Edge Part Type Library
WeldBeadModel Object Members
Overview 
Public Methods
Public Method SaveBodySaves the body of this model to the specified document in the specified format
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BodyReturns the Body object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
See Also

WeldBeadModel Object