Solid Edge Part Type Library
UserDefinedPattern Object
Members 
Description
A mechanism for grouping features that is independent of the positioning of the features.
Object Model
UserDefinedPattern ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
It differs from the CircularPattern2d and RectangularPattern2d objects in that it does not define any positioning of the features in the pattern. A UserDefinedPattern is used when the user defines multiple holes in the Hole command.
See Also

UserDefinedPattern Members