Solid Edge Part Type Library
Add Method
Description
Syntax
Visual Basic
Public Function Add( _
   ByVal NumOfBodies As Long, _
   ByRef BodyArray() As Object _
) As ToggleToDesign
Parameters
NumOfBodies
BodyArray
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()

        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objConstructions As SolidEdgePart.Constructions = Nothing
        Dim objToggleToDesigns As SolidEdgePart.ToggleToDesigns = Nothing
        Dim objToggleToDesign As SolidEdgePart.ToggleToDesign = Nothing
        Dim BodyArray(1) As Object

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument
            objModels = objPartDocument.Models
            objConstructions = objPartDocument.Constructions
            objToggleToDesigns = objModels.ToggleToDesigns

            BodyArray(1) = Nothing
            BodyArray(1) = objConstructions.Item(1).Body

            objToggleToDesign = objToggleToDesigns.Add(1, BodyArray)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

ToggleToDesigns Collection  | ToggleToDesigns Members  | Solid Edge ST5 - What's New