Solid Edge Part Type Library
GetSettingsList Method
Description
Get various settings options from a study owner.
Syntax
Visual Basic
Public Sub GetSettingsList( _
   ByRef varSettingsArray As Variant _
) 
Parameters
varSettingsArray
Remarks
In analysis results environment we could create several display settings similar to assembly configurations. All these settings are stored per document. These are present in a vector under studyowner object.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim vOriginArray(1) As Object

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument

            objStudyOwner = objAssemblyDocument.StudyOwner
            vOriginArray(0) = 0
            objStudyOwner.GetSettingsList(vOriginArray)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

StudyOwner Collection  | StudyOwner Members  | Solid Edge ST3 - What's New