Solid Edge Part Type Library
Add Method
Description
Syntax
Visual Basic
Public Function Add( _
   ByVal nNumTargets As Long, _
   ByRef TargetArray() As Object, _
   ByVal nNumTools As Long, _
   ByRef ToolsArray() As Object, _
   ByVal TargetDesignBodyOption As SETargetDesignBodyOption, _
   ByVal TargetConstructionBodyOption As SETargetConstructionBodyOption _
) As Split
Parameters
nNumTargets
TargetArray
nNumTools
ToolsArray
TargetDesignBodyOption
ValueDescription
igCreateMultipleDesignBodiesOnNonManifoldOption
igFailOnNonManifoldOption
TargetConstructionBodyOption
ValueDescription
igCreateMultipleConstructionBodiesOnNonManifoldOption
igCreateSingleConstructionGeneralBodyOnNonManifoldOption
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objSplits As SolidEdgePart.Splits = Nothing
        Dim objSplit As SolidEdgePart.Split = Nothing
        Dim objTargetBodySplit(5) As Object
        Dim objToolBodySplit(5) As Object

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objModels = objPartDocument.Models

            objTargetBodySplit(0) = objModels.Item(1).Body
            objToolBodySplit(0) = objModels.Item(2).Body

            objModel = objModels.Item(1)
            objSplits = objModel.Splits

            objSplit = objSplits.Add(1, objTargetBodySplit, 1, objToolBodySplit,
                                           SolidEdgePart.SETargetDesignBodyOption.igCreateMultipleDesignBodiesOnNonManifoldOption,
                                            SolidEdgePart.SETargetConstructionBodyOption.igCreateMultipleConstructionBodiesOnNonManifoldOption)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Splits Collection  | Splits Members  | Solid Edge ST5 - What's New