Solid Edge Part Type Library
SplitFaces Collection Members
Overview 
Public Methods
Public Method AddAdds an occurrence of the referenced object.
Public Method AreValidTargetsReturns True if the specified target elements are valid input for a SplitFace feature.
Public Method IsValidToolReturns True if the specified splitting element is valid for the specified target surfaces.
Public Method ItemThe items in a collection.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property ParentReturns the parent object for the referenced object.
See Also

SplitFaces Collection