Solid Edge Part Type Library
PlaceFeatureLibrary Method
Source document from which features are to be copied into target document.
Destination RefPlace in target document.
X Origin placement in target document.
Y Origin placement in target document.
Z Origin placement in target document.
Returned array of Features that were added to target document.
Description
Places features from an existing document into the current document.
Syntax
Visual Basic
Public Sub PlaceFeatureLibrary( _
   ByVal LibName As String, _
   ByVal RefPlane As Object, _
   ByVal Xorigin As Double, _
   ByVal Yorigin As Double, _
   ByVal Zorigin As Double, _
   ByRef Features() As Object _
) 
Parameters
LibName
Source document from which features are to be copied into target document.
RefPlane
Destination RefPlace in target document.
Xorigin
X Origin placement in target document.
Yorigin
Y Origin placement in target document.
Zorigin
Z Origin placement in target document.
Features
Returned array of Features that were added to target document.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objTrainingFolder As DirectoryInfo = Nothing
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objPartDocument As SolidEdgePart.SheetMetalDocument = Nothing
        Dim objRefPlanes As SolidEdgePart.RefPlanes = Nothing
        Dim objRefPlane As SolidEdgePart.RefPlane = Nothing
        Dim objFeatures As Array
        Dim objFeature As Object
        Dim featureType As SolidEdgePart.FeatureTypeConstants

        Try
            OleMessageFilter.Register()

            objTrainingFolder = GetTrainingFolder()
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents
            objPartDocument = objDocuments.Add("SolidEdge.SheetMetalDocument")
            objRefPlanes = objPartDocument.RefPlanes
            objFeatures = Array.CreateInstance(GetType(System.Object), 0)

            objRefPlane = objRefPlanes.Item(1)
            objPartDocument.PlaceFeatureLibrary(Path.Combine(objTrainingFolder.FullName, "bar.par"), objRefPlane, 0.0, 0.0, 0.0, objFeatures)

            For Each objFeature In objFeatures
                featureType = objFeature.Type
                Select Case featureType
                    Case SolidEdgePart.FeatureTypeConstants.igAssemblyWeldmentObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igAssemblyWeldmentObject
                    Case SolidEdgePart.FeatureTypeConstants.igBeadFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBeadFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igBendFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBendFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igBlueSurfFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBlueSurfFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igBodyFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBodyFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igBooleanFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBooleanFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igBreakCornerFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igBreakCornerFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igChamferFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igChamferFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igCloseCornerFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igCloseCornerFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igContourFlangeFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igContourFlangeFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igCoordinateSystemFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igCoordinateSystemFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igCopiedPartFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igCopiedPartFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igCopyConstructionObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igCopyConstructionObject
                    Case SolidEdgePart.FeatureTypeConstants.igCopySurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igCopySurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igDeleteBlendFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDeleteBlendFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDeleteFaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDeleteFaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDeleteHoleFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDeleteHoleFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDeleteRegionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDeleteRegionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDerivedCurveObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDerivedCurveObject
                    Case SolidEdgePart.FeatureTypeConstants.igDimpleFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDimpleFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDraftFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDraftFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igDrawnCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igDrawnCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igEtchFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igEtchFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igExtendSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igExtendSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igExtrudedCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igExtrudedCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igExtrudedProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igExtrudedProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igExtrudedSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igExtrudedSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igFaceMoveObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igFaceMoveObject
                    Case SolidEdgePart.FeatureTypeConstants.igFaceOffsetObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igFaceOffsetObject
                    Case SolidEdgePart.FeatureTypeConstants.igFaceRotateObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igFaceRotateObject
                    Case SolidEdgePart.FeatureTypeConstants.igFilletWeldFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igFilletWeldFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igFlangeFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igFlangeFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igGussetFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igGussetFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igHelixCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igHelixCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igHelixProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igHelixProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igHoleFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igHoleFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igInterpartConstructionObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igInterpartConstructionObject
                    Case SolidEdgePart.FeatureTypeConstants.igIntersectionCurveObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igIntersectionCurveObject
                    Case SolidEdgePart.FeatureTypeConstants.igIntersectionPointObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igIntersectionPointObject
                    Case SolidEdgePart.FeatureTypeConstants.igJogFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igJogFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLabelWeldFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLabelWeldFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLipFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLipFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLiveSectionObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLiveSectionObject
                    Case SolidEdgePart.FeatureTypeConstants.igLoftedCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLoftedCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLoftedFlangeFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLoftedFlangeFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLoftedProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLoftedProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLoftedSurfaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLoftedSurfaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igLouverFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igLouverFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igMatchFlangeFaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igMatchFlangeFaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igMidSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igMidSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igMirrorCopyFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igMirrorCopyFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igMirrorCopyGeometryObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igMirrorCopyGeometryObject
                    Case SolidEdgePart.FeatureTypeConstants.igMirrorPartFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igMirrorPartFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igModelCopyFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igModelCopyFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igNormalCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igNormalCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igNormalToFaceCutoutObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igNormalToFaceCutoutObject
                    Case SolidEdgePart.FeatureTypeConstants.igNormalToFaceProtrusionObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igNormalToFaceProtrusionObject
                    Case SolidEdgePart.FeatureTypeConstants.igOffsetSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igOffsetSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igPartingSplitFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igPartingSplitFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igPartingSurfaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igPartingSurfaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igPatternCopyGeometryObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igPatternCopyGeometryObject
                    Case SolidEdgePart.FeatureTypeConstants.igPatternFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igPatternFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igPatternPartFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igPatternPartFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igProjectCurveObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igProjectCurveObject
                    Case SolidEdgePart.FeatureTypeConstants.igRebendFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRebendFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igReplaceFaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igReplaceFaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igResizeBendObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igResizeBendObject
                    Case SolidEdgePart.FeatureTypeConstants.igResizeHoleObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igResizeHoleObject
                    Case SolidEdgePart.FeatureTypeConstants.igResizeRoundObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igResizeRoundObject
                    Case SolidEdgePart.FeatureTypeConstants.igRevolvedCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRevolvedCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igRevolvedProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRevolvedProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igRevolvedSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRevolvedSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igRibFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRibFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igRoundFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igRoundFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igSplitCurveObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSplitCurveObject
                    Case SolidEdgePart.FeatureTypeConstants.igSplitFaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSplitFaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igStitchSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igStitchSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igSurfaceByBoundaryObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSurfaceByBoundaryObject
                    Case SolidEdgePart.FeatureTypeConstants.igSweptCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSweptCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igSweptProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSweptProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igSweptSurfaceFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igSweptSurfaceFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igTabFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igTabFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igThickenFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igThickenFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igThinRegionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igThinRegionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igThinwallFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igThinwallFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igTrimSurfaceObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igTrimSurfaceObject
                    Case SolidEdgePart.FeatureTypeConstants.igTubeFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igTubeFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igUnbendFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igUnbendFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igUserDefinedPatternFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igUserDefinedPatternFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igVentFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igVentFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWebNetworkFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWebNetworkFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldBeadByExtrudedProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldBeadByExtrudedProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldBeadByRevolvedProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldBeadByRevolvedProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldBeadBySweptProtrusionFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldBeadBySweptProtrusionFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldChamferFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldChamferFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldExtrudedCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldExtrudedCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldHoleFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldHoleFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldMirrorFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldMirrorFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldPatternFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldPatternFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldRevolvedCutoutFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldRevolvedCutoutFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWeldRoundFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWeldRoundFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWireFeatureObject
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWireFeatureObject
                    Case SolidEdgePart.FeatureTypeConstants.igWrapSketch
                        'Handle type SolidEdgePart.FeatureTypeConstants.igWrapSketch
                End Select
            Next
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub

    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function
End Module
See Also

SheetMetalDocument Object  | SheetMetalDocument Members  | Solid Edge V17 - What's New