Solid Edge Part Type Library
NormalDistance Method
The first element.
The second element.
The true distance between Element1 and Element2.
The apparent distance between Element1 and Element2.
The X axis component of the true normal distance.
The Y axis component of the true normal distance.
The Z axis component of the true normal distance.
Specifies the coordinate system that defines one of the elements. If you include CoordinateSystem input, the returned values are relative to the coordinate system.
Description
Measures the normal distance between lines or planes.
Syntax
Visual Basic
Public Sub NormalDistance( _
   ByVal Element1 As Object, _
   ByVal Element2 As Object, _
   ByRef TrueDistance As Double, _
   ByRef ApparentDistance As Double, _
   ByRef DeltaX As Double, _
   ByRef DeltaY As Double, _
   ByRef DeltaZ As Double, _
   Optional ByVal CoordinateSystem As Variant _
) 
Parameters
Element1
The first element.
Element2
The second element.
TrueDistance
The true distance between Element1 and Element2.
ApparentDistance
The apparent distance between Element1 and Element2.
DeltaX
The X axis component of the true normal distance.
DeltaY
The Y axis component of the true normal distance.
DeltaZ
The Z axis component of the true normal distance.
CoordinateSystem
Specifies the coordinate system that defines one of the elements. If you include CoordinateSystem input, the returned values are relative to the coordinate system.
See Also

SheetMetalDocument Object  | SheetMetalDocument Members