Solid Edge Part Type Library
Rounds Collection Members
Overview 
Public Methods
Public Method AddAdds an occurrence of the referenced object.
Public Method AddBlendCreates a blend between edges, faces, or a combination of the two.
Public Method AddSurfaceBlendCreates a blend between 2 faces of construction surfaces.
Public Method AddVariableAdds a variable-radius Round feature.
Public Method ItemThe items in a collection.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property ParentReturns the parent object for the referenced object.
See Also

Rounds Collection