Solid Edge Part Type Library
Rib Object
Members 
Description
A feature that is defined by a profile curve that is projected to intersect a part.
Object Model
Rib ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
A rib/web is a feature that is defined by a profile curve that is projected to intersect a part. A valid rib/web must intersect the part in at least one location. A true rib must intersect the part in at least two locations. A web can intersect the part at only one point and still be valid. Because the Rib object is a material extension, it cannot exist alone. Therefore, it must be a material addition to an existing part.
See Also

Rib Members