Solid Edge Part Type Library
RevolvedProtrusion Object
Members 
Description
A feature that is defined using an open or closed profile that revolves about an axis.
Object Model
RevolvedProtrusion ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
A Revolved Protrusion is a feature that is defined using an open or closed profile that revolves about a Reference Axis (a RefAxis object). The volume that is defined by the revolution is added to the solid.
See Also

RevolvedProtrusion Members