Solid Edge Part Type Library
GetProperties Method
Description
Get results properties.
Syntax
Visual Basic
Public Sub GetProperties( _
   ByRef pdwProps As ULong _
) 
Parameters
pdwProps
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objResultsOwner As SolidEdgePart.ResultsOwner = Nothing
        Dim nResProp As UInt32 = 0

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)
            objStudy.GetResultsOwner(objResultsOwner)

            objResultsOwner.GetProperties(nResProp)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

ResultsOwner Object  | ResultsOwner Members  | Solid Edge ST3 - What's New