Solid Edge Part Type Library
RefAxis Object
Members 
Description
Defines the axis of conical-based features.
Object Model
RefAxis ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Remarks
The RefAxis object is a linear object that defines the axis of cylindrical-based features: revolved protrusions, revolved cutouts, and holes. For revolved features, a RefAxis object is a parent of the feature and is provided as input when creating the feature. For Hole features, a RefAxis object is a resulting child of the feature and can be referenced when creating other revolved features.
See Also

RefAxis Members