Solid Edge Part Type Library
SetEdgeTangencyTypes Method
Number of edges.
Array of edges.
Description
Set specific tangency types on redefine surface edges.
Syntax
Visual Basic
Public Sub SetEdgeTangencyTypes( _
   ByVal NumberOfEdgesAndTypes As Long, _
   ByRef BoundaryEdgesArray() As Object, _
   ByRef TangencyTypeArray() As RedefineFaceTangencyType _
) 
Parameters
NumberOfEdgesAndTypes
Number of edges.
BoundaryEdgesArray
Array of edges.
TangencyTypeArray
ValueDescription
igRedefineFaceCurvatureContinuous
igRedefineFaceNatural
igRedefineFaceNormalToPlane
igRedefineFaceTangentContinuous
Remarks

All the edges need not be input to it. Only the edges for which tangency types is to be changed can be sent.

NOTE: We must roll to previous feature before we get/set tangency types for edges. This is because the tangency is set on edges which are present before creating redefine feature. Also, roll to current feature after setting tangency types to see the changes.

See Also

RedefineFace Object  | RedefineFace Members