Solid Edge Part Type Library > RedefineFace Object : InsertUVCurve Method |
Visual Basic |
---|
Public Sub InsertUVCurve( _ ByVal NumberOfFaces As Long, _ ByRef FacesArray() As Object, _ ByRef IsUCurve() As Boolean, _ ByRef UOrVParameter() As Double, _ ByVal UsePiercePoints As Boolean _ ) |
If UV curve is to be inserted across multiple faces, all the needed faces, corresponding parameters and Boolean values denoting whether to consider U or V line at the parameter should be input.
NOTE: We must roll to previous feature before we insert UV curve. This is because the UV curve is created on input faces to redefine feature.