Solid Edge Part Type Library
GetXYZLocationsOfMinValue Method
Description
Get minimum values at X, Y and Z locations.
Syntax
Visual Basic
Public Sub GetXYZLocationsOfMinValue( _
   ByRef nValAtX As Double, _
   ByRef nValAtY As Double, _
   ByRef nValAtZ As Double _
) 
Parameters
nValAtX
nValAtY
nValAtZ
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objPlotsOwner As SolidEdgePart.PlotsOwner = Nothing
        Dim objPlot As SolidEdgePart.Plot = Nothing
        Dim dValAtX As Double = 0.0
        Dim dValAtY As Double = 0.0
        Dim dValAtZ As Double = 0.0

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)

            ' This will give us active plotsowner.
            objStudy.GetPlotsOwner(objPlotsOwner)

            ' Get active plot object
            objPlotsOwner.GetActivePlot(objPlot)

            objPlot.GetXYZLocationsOfMinValue(dValAtX, dValAtY, dValAtZ)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Plot Object  | Plot Members  | Solid Edge ST3 - What's New