Solid Edge Part Type Library
PatternCopyGeometry Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method DropParentsRemoves associative connection with parents, so that it can not edited or recomputed.
Public Method ExactRangeThis method sets the exact range parameters for the referenced object.
Public Method GetCurve1Curves
Public Method GetCurve1Data
Public Method GetCurve2CurvesThis method returns curve data for the path curve for the referenced object.
Public Method GetCurve2DataThis method returns data parameters for the path curve for the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetEntitiesThis method returns the entities (curves or surfaces) for the referenced object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method GetTransformTypeThis method returns the transformation type for the referenced object.
Public Method InsertOccurrenceThis method inserts a pattern occurrence for the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetCurve1CurvesThis method sets curve data for the select curve for the referenced object.
Public Method SetCurve1DataThis method sets data parameters for the select curve for the referenced object.
Public Method SetCurve2CurvesThis method sets curve data for the path curve for the referenced object.
Public Method SetCurve2DataThis method sets data parameters for the path curve for the referenced object.
Public Method SetEntitiesThis method sets the entities (curves or surfaces) for the referenced object.
Public Method SetStyleSets the feature style.
Public Method SetTransformTypeThis method sets the transformation type for the referenced object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property NumberOfOccurrencesReturns the number of occurrences.
Public Property OccurrenceEdgesReturns the edges that belong to an occurrence of the referenced Pattern object.
Public Property OccurrenceFacesReturns the faces that belong to an occurrence of the referenced Pattern object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PatternPlaneReturns the PatternPlane object for the referenced object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property ReferenceOccurrence
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressedSpecifies whether or not the referenced pattern object is suppressed.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TransformsReturns a read-only variant.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

PatternCopyGeometry Object