Solid Edge Part Type Library
PartingSplit Object
Members 
Description
An occurrence of a parting split feature.
Object Model
PartingSplit ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
A parting split is represented by a curve that splits a set of faces along the silhouette edges of a part.
See Also

PartingSplit Members