Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BottomCapMethod | Sets and returns the bottom cap method of the part weldment feature. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndCapMethod | Sets and returns the end cap method of the part weldment feature. |
EndOffsetValue | end offset value of the feature. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LabelWeldData | Returns a LabelWeldData object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
StartCapMethod | Sets and returns the start cap method of the part weldment feature. |
StartOffsetValue | start offset value of the feature. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | |
TopCapMethod | Sets and returns the top cap method of the part weldment feature. |
Type | Specifies the type of the object being referenced. |