Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BaseWidthOrThickness | Sets and returns either the base width or thickness of the feature. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LabelWeldData | Returns a LabelWeldData object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
SetbackMethod | Returns the setback method of the weldment feature. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | |
TargetWidth | Sets and returns the target width of the feature. |
Type | Specifies the type of the object being referenced. |