Solid Edge Part Type Library
RefAxes Property
Description
Returns the RefAxes collection object for the referenced document object.
Property type
Read-only property
Syntax
Visual Basic
Public Property RefAxes As RefAxes
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objRefAxes As SolidEdgePart.RefAxes
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the collection of reference axes on the part document
    Set objRefAxes = objDoc.RefAxes
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objRefAxes = Nothing
End Sub
See Also

PartDocument Object  | PartDocument Members