Solid Edge Part Type Library
ModelingMode Property
Description
The property transitions the document between Synchronous and Ordered as is done in the UI via Pathfinder or a context menu.
Property type
Read-write property
Syntax
Visual Basic
Public Property ModelingMode As ModelingModeConstants
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            ' Demonstrate transitioning to different ModelingMode.
            Select Case objPartDocument.ModelingMode
                Case SolidEdgePart.ModelingModeConstants.seModelingModeOrdered
                    objPartDocument.ModelingMode = SolidEdgePart.ModelingModeConstants.seModelingModeSynchronous
                Case SolidEdgePart.ModelingModeConstants.seModelingModeSynchronous
                    objPartDocument.ModelingMode = SolidEdgePart.ModelingModeConstants.seModelingModeOrdered
            End Select

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

PartDocument Object  | PartDocument Members  | Solid Edge ST3 - What's New