Solid Edge Part Type Library
DeleteFrameDefineOriginAndOrientation Method
Description
Deletes Origin Point for Frame.
Syntax
Visual Basic
Public Sub DeleteFrameDefineOriginAndOrientation() 
Example
Public Class Frame_Define_Origin_and_Orientation

    Private Sub FrameDefineOriginAndOrientation_Click(sender As System.Object, e As System.EventArgs) Handles FrameDefineOriginAndOrientation.Click
        Dim objPartDoc As SolidEdgePart.PartDocument = Nothing
        Dim objProfile As SolidEdgePart.Profile = Nothing
        Dim sketch As SolidEdgePart.Sketch = Nothing
        Dim objPoint As SolidEdgeFrameworkSupport.Point2d = Nothing
        Dim objOrientation As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPointOut As SolidEdgeFrameworkSupport.Point2d = Nothing
        Dim objOrientationOut As SolidEdgeFrameworkSupport.Line2d = Nothing

        Try
            ' Create/get the application with specific settings 
            objApplication = GetObject(, "SolidEdge.Application")

            'Open the Document mentioned in the Doc Files.
            ' OR User can create a part file having a sketch
            objPartDoc = objApplication.Documents.Open("C:\FrameDefineOriginInSketch.par")

            If objPartDoc Is Nothing Then
                MsgBox("Could not open document ")
            End If

            ' Input Edges
            sketch = objPartDoc.Sketches.Item(1)
            objProfile = sketch.Profile

            'Get Input Edge
            objOrientation = objProfile.Lines2d.Item(3)
            'Get Input Point
            objPoint = objProfile.Points2d.Item(1)
            'Set Frame Define Origin And Orientation
            objPartDoc.SetFrameDefineOriginAndOrientation(objOrientation, objPoint)
            'Get Frame Define Origin And Orientation
            objPartDoc.GetFrameDefineOriginAndOrientation(objOrientationOut, objPointOut)
            'Delete Frame Define Origin And Orientation
            objPartDoc.DeleteFrameDefineOriginAndOrientation()
            objOrientationOut = Nothing
            objPointOut = Nothing
        Catch ex As Exception
            MsgBox(ex.Message)
        End Try
    End Sub


End Class
See Also

PartDocument Object  | PartDocument Members