Solid Edge Part Type Library
DeActivateReflectivePlane Method
Description
This method will turn OFF reflective plane command which is similar to unchecked box at ribbon bar of Inspect Tab in Solid Edge UI.
Syntax
Visual Basic
Public Sub DeActivateReflectivePlane() 
Example
Public Class Form1

    Private Sub btnReflectivePlane_Click(sender As System.Object, e As System.EventArgs) Handles btnReflectivePlane.Click
        Dim objPartDoc As SolidEdgePart.PartDocument = Nothing
        Dim objProfile As SolidEdgePart.Profile = Nothing
        Dim sketch As SolidEdgePart.Sketch = Nothing
        Dim objPoint As SolidEdgeFrameworkSupport.Point2d = Nothing
        Dim objOrientation As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPointOut As SolidEdgeFrameworkSupport.Point2d = Nothing
        Dim objOrientationOut As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim bStatus As Boolean = False
        Dim dDistance As Double = 0
        Dim iTransparency As Integer = 30

        Try

            ' Create/get the application with specific settings
            objApplication = GetObject(, "SolidEdge.Application")
            If objApplication Is Nothing Then
                MessageBox.Show("Could not get application.")
            End If

            ' open the document mentioned in the doc files.
            objPartDoc = objApplication.Documents.Open("C:\ReflectivePlane.par")
            If objPartDoc Is Nothing Then
                MessageBox.Show("Could not open document ")
            End If

            objPartDoc.ActivateReflectivePlane()

            objPartDoc.SetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igTopPlane, True, 0.3)
            objPartDoc.SetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igRightPlane, True, 0.4)
            objPartDoc.SetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igFrontPlane, True, 0.5)

            objPartDoc.GetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igTopPlane, bStatus, dDistance)
            objPartDoc.GetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igRightPlane, bStatus, dDistance)
            objPartDoc.GetReflectivePlane(SolidEdgePart.ReflectivePlaneConstants.igFrontPlane, bStatus, dDistance)

            objPartDoc.SetReflectivePlaneTransparency(True, iTransparency)
            objPartDoc.GetReflectivePlaneTransparency(bStatus, iTransparency)

            'objPartDoc.DeActivateReflectivePlane()

            If objPartDoc Is Nothing Then
                objPartDoc.Close(False)
                objPartDoc = Nothing
            End If

        Catch ex As Exception
            MsgBox(ex.Message)
        End Try
    End Sub
End Class
See Also

PartDocument Object  | PartDocument Members