Solid Edge Part Type Library
PMIModelStateConstants Enumeration
Description
Enumerates the model states – will be used to get PMI dimensions and annotations based on model state through the function PMI_ByModelState()
Members
MemberValueDescription
seDesignModelState1Specifies the DESIGN model state - default value when getting PMI dimensions and annotations through the function PMI_ByModelState()
seFlatModelState2Specifies the FLAT model state - will be used to get PMI dimensions and annotations based on flat model state through the function PMI_ByModelState()
seSimplifyModelState3Specifies the SIMPLIFY model state - will be used to get PMI dimensions and annotations based on simplify model state through the function PMI_ByModelState()
See Also

Solid Edge ST2 - What's New