Solid Edge Part Type Library
OverProp Object Members
Overview 
Public Methods
Public Method DeleteDelete a particular OverrideProperty object.
Public Method GetGeometriesGet an array of geometry objects on which the override property has been applied.
Public Method GetMaterialGet material applied on the the face selected for override property.
Public Method GetPlatePropIDGet Prop id.
Public Method SetGeometriesSet edges/faces/vertices etc as geometry to apply override property on.
Public Method SetMaterialSet material on the face selected for applying override property.
Public Method SetPlatePropIDSet Prop id.
See Also

OverProp Object  | Solid Edge ST4 - What's New