Solid Edge Part Type Library
NormalToFaceCutout Object
Members 
Description
A cutout with closed curves that follows a path normal to the faces on which the curves lie.
Object Model
NormalToFaceCutout ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
The NormalToFaceCutout object represents an occurrence of a cutout feature that is normal to a face in a Part or Sheet Metal document.
See Also

NormalToFaceCutout Members