Solid Edge Part Type Library
MeasureVariable Object Members
Overview 
Public Methods
Public Method DeleteDeletes the Measure variable object.
Public Method GetGeometriesReturns the Measure variable input geometries.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property MeasureTypeReturns the Measure variable type.
Public Property ParentReturns the parent object for the referenced object.
Public Property ValueReturns the Measure variable value.
Public Property ValueTypeReturns the Measure variable value type.
See Also

MeasureVariable Object