Imports System.IO
Imports System.Runtime.InteropServices
Module Example
<STAThread()> _
Sub Main()
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
Dim objStudy As SolidEdgePart.Study = Nothing
Dim objLoadOwner As SolidEdgePart.LoadOwner = Nothing
Dim objLoad As SolidEdgePart.Load = Nothing
Dim eLoadDirection As SolidEdgePart.LoadSymbDirOptsEnum_Auto
Dim eLoadType As SolidEdgePart.FEALoadTypeEnum_Auto
Dim dLoadValue As Double = 2500000
Dim dLoadDirX As Double = -0.0
Dim dLoadDirY As Double = 1.0
Dim dLoadDirZ As Double = -0.0
Dim dLoadPosX As Double = -0.0754203151729549
Dim dLoadPosY As Double = 0.015441908335819984
Dim dLoadPosZ As Double = 0.056796356131827666
Dim dSpacingFactor As Double = 0.11
Dim dSizeFactor As Double = 0.24200000000000002
Dim dSteeringWheelLen As Double = 0.020253310860972911
Dim dwLoadProps As UInt32 = 0
Dim dLoadSymSpacing As Double = 0.016464634271235477
Dim dLoadSymSize As Double = 0.036222195396718053
Dim ColorLoadSymbol As UInt32 = 16736256
Dim ColorLoadSymbolAngAcc As UInt32 = 8388673
Try
OleMessageFilter.Register()
' Connect to Solid Edge
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
objPartDocument = objApplication.ActiveDocument
objStudyOwner = objPartDocument.StudyOwner
objStudy = objStudyOwner.Item(1)
objStudy.GetLoadOwner(objLoadOwner)
objLoad = objLoadOwner.Item(1)
eLoadDirection = SolidEdgePart.LoadSymbDirOptsEnum_Auto.eLoadDirForCnstr_Auto
eLoadType = SolidEdgePart.FEALoadTypeEnum_Auto.eLoadTypeForce_Auto
objLoad.SetLoadOptions(eLoadType, _
dLoadValue, _
0, _
eLoadDirection, _
dLoadDirX, _
dLoadDirY, _
dLoadDirZ, _
dLoadPosX, _
dLoadPosY, _
dLoadPosZ, _
ColorLoadSymbol, _
ColorLoadSymbolAngAcc, _
dSpacingFactor, _
dSizeFactor, _
dSteeringWheelLen, _
dwLoadProps, _
dLoadSymSpacing, _
dLoadSymSize)
Catch ex As Exception
Console.WriteLine(ex.Message)
Finally
OleMessageFilter.Revoke()
End Try
End Sub
End Module