Solid Edge Part Type Library
SetGeometries Method
Description
Set edges/faces/vertices etc as geometry to apply load on.
Syntax
Visual Basic
Public Sub SetGeometries( _
   ByRef arrStudyGeomeProxies() As Object _
) 
Parameters
arrStudyGeomeProxies
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objLoadOwner As SolidEdgePart.LoadOwner = Nothing
        Dim objLoad As SolidEdgePart.Load = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objExtProt As SolidEdgePart.ExtrudedProtrusion = Nothing
        Dim objFaces As SolidEdgeGeometry.Faces = Nothing
        Dim objFaceArray(2) As SolidEdgeGeometry.Face

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)
            objStudy.GetLoadOwner(objLoadOwner)
            objLoad = objLoadOwner.Item(1)

            ' Get Model
            objModel = objPartDocument.Models.Item(1)

            ' Get Protrusion.
            objExtProt = objModel.ExtrudedProtrusions.Item(1)

            ' Get faces collection
            objFaces = objExtProt.Faces(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)

            objFaceArray(0) = objFaces.Item(2)
            objFaceArray(1) = objFaces.Item(3)
            objFaceArray(2) = objFaces.Item(4)

            'Set geometries on study
            objLoad.SetGeometries(objFaceArray)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Load Object  | Load Members  | Solid Edge ST3 - What's New