Solid Edge Part Type Library
Hole Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetProfilesReturns the profiles associated with the referenced feature object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetProfilesSets the profiles associated with the referenced feature object.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BottomCapReturns the bottom face of a feature object.
Public Property DepthSets and returns the distance that the referenced object extends or removes material from a solid.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property DraftAngleSets and returns the angle at which the hole is angled from the normal of the reference plane.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property ExtentSideSets and returns the reference plane side for the referenced object.
Public Property ExtentTypeSets and returns the extent type for the referenced object.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property FromPlaneSets and returns the RefPlane object from which a protrusion, hole, or cutout feature begins.
Public Property HoleDataReturns the HoleData object for the referenced Hole object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeTypeReturns the modeling mode of the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property SideFacesReturns a collection of all the side faces for the referenced feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TopCapReturns the top face of the referenced feature object.
Public Property ToPlaneSets and returns the RefPlane object from which a protrusion, hole, or cutout feature terminates.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

Hole Object