Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Blanks | Returns the Blanks collection |
Body | Returns the Body object for the referenced object. |
CutSizeViolation | This read-only property sets the limit for the flat pattern cut size. If this limit is exceeded alarm icon is displayed adjacent to the flat pattern entry in PathFinder. |
DeleteBlends | Represents a collection of delete blend objects. |
DeleteFaces | Represents a collection of delete face objects. |
DeleteHoles | Represents a collection of delete hole objects. |
DeleteRegions | Represents a collection of delete region objects. |
DisplayName | This read-only String property returns the display name for the referenced object. |
Document | Returns the document to which the referenced object belongs. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Etches | Returns the Etches collection object for the referenced Model. |
ExtrudedCutouts | Returns the ExtrudedCutouts collection object for the referenced Model. |
ExtrudedProtrusions | Returns the ExtrudedProtrusions collection object for the referenced Model. |
Features | Returns the Features collection object for the referenced Model. |
FlatPatterns | Returns the FlatPattern collection for the referenced Model. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsModelActive | This read-only property specifies if the model is active in Solid Edge. |
IsUpToDate | Finds the uptodate of the referenced Model. |
ModelRecomputeEvents | Returns the ModelRecomputeEvents object for the referenced Model object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
RevolvedCutouts | Returns the RevolvedCutouts collection object for the referenced Model. |
RevolvedProtrusions | Returns the RevolvedProtrusions collection object for the referenced Model. |
SystemName | This read-only String property returns the system name for the referenced object. |
Tabs | |