Solid Edge Part Type Library
SetGeometries Method
Description
Set edges/faces/vertices etc as geometry to apply constraint on.
Syntax
Visual Basic
Public Sub SetGeometries( _
   ByRef arrStudyGeomeProxies() As Object _
) 
Parameters
arrStudyGeomeProxies
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objConstraintOwner As SolidEdgePart.ConstraintOwner = Nothing
        Dim objConstraint As SolidEdgePart.FEAConstraint = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objExtProt As SolidEdgePart.ExtrudedProtrusion = Nothing
        Dim objEdges As SolidEdgeGeometry.Edges = Nothing
        Dim objProxiesArray(1) As Object

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)
            objStudy.GetConstraintOwner(objConstraintOwner)
            objConstraint = objConstraintOwner.Item(1)

            ' Get Model
            objModel = objPartDocument.Models.Item(1)

            ' Get Protrusion.
            objExtProt = objModel.ExtrudedProtrusions.Item(1)

            ' Get Edges Colection
            objEdges = objExtProt.Edges(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)

            ' Store edge proxies in vector
            objProxiesArray(0) = objEdges.Item(3)
            objProxiesArray(1) = objEdges.Item(4)

            objConstraint.SetGeometries(objProxiesArray)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

FEAConstraint Object  | FEAConstraint Members  | Solid Edge ST3 - What's New