Solid Edge Part Type Library
GetConstraintOptions Method
Constraint Type
Constraint Direction
X Direction
Y Direction
Z Direction
X Direction
Y Direction
Z Direction
Color of the symbols
Symbol spacing factor
Symbol size factor
Steering wheel length
Constraint properties
Symbol spacing factor
Constraint symbol size
Description
Get values for various options parameters like constraint type, properties, symbol size/spacing etc.
Syntax
Visual Basic
Public Sub GetConstraintOptions( _
   ByRef eConstraintType As FEAConstraintTypeEnum_Auto, _
   ByRef eConstraintDir As LoadSymbDirOptsEnum_Auto, _
   ByRef x As Double, _
   ByRef y As Double, _
   ByRef z As Double, _
   ByRef xx As Double, _
   ByRef yy As Double, _
   ByRef zz As Double, _
   ByRef colorConstraintSymbol As ULong, _
   ByRef dSpacingFactor As Double, _
   ByRef dSizeFactor As Double, _
   ByRef dSteeringWheelLen As Double, _
   ByRef dwConstraintProps As ULong, _
   ByRef dwConstraintSymSpacing As Double, _
   ByRef dConstraintSymSize As Double _
) 
Parameters
eConstraintType
ValueDescription
eCnstrTypeCylindrical_Auto 
eCnstrTypeFixed_Auto 
eCnstrTypeNone_Auto 
eCnstrTypeNoRotation_Auto 
eCnstrTypePinned_Auto 
eCnstrTypeSlidingAlongSurface_Auto 
eCnstrTypeUserDefined_Auto 
Constraint Type
eConstraintDir
ValueDescription
eLoadDirAboutAxis_Auto 
eLoadDirAlongVec_Auto 
eLoadDirCentrifugal_Auto 
eLoadDirComponents_Auto 
eLoadDirDefault_Auto 
eLoadDirForCnstr_Auto 
eLoadDirGravity_Auto 
eLoadDirHeatFlux_Auto 
eLoadDirNormalToFace_Auto 
eLoadDirTorque_Auto 
Constraint Direction
x
X Direction
y
Y Direction
z
Z Direction
xx
X Direction
yy
Y Direction
zz
Z Direction
colorConstraintSymbol
Color of the symbols
dSpacingFactor
Symbol spacing factor
dSizeFactor
Symbol size factor
dSteeringWheelLen
Steering wheel length
dwConstraintProps
Constraint properties
dwConstraintSymSpacing
Symbol spacing factor
dConstraintSymSize
Constraint symbol size
See Also

FEAConstraint Object  | FEAConstraint Members  | Solid Edge ST3 - What's New