Solid Edge Part Type Library
EmbossFeature Object Members
Overview 
Public Methods
Public Method DeleteDeletes the Emboss Feature.
Public Method EditCan send new values to feature and it will be edited accordingly.
Public Method ExactRange
Public Method GetEmbossToolBodiesGet Emboss Bodies.
Public Method GetStatusExReturns the status of the specified object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetEmbossToolBodies
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property Clearance
Public Property DieRadius
Public Property DieRounding
Public Property DisplayName
Public Property EdgebarName
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property EmbossTarget
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PunchSideRadius
Public Property PunchSideRounding
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property Side
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemName
Public Property Thicken
Public Property Thickness
Public Property TypeSpecifies the type of the object being referenced.
See Also

EmbossFeature Object