Solid Edge Part Type Library
Draft Object
Members 
Description
A material treatment to an existing face or set of faces.
Object Model
Draft ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
It cannot exist independently. Instead, this object modifies existing faces by angling (drafting) them inward or outward. A Draft object can replace a single face or a set of faces. If the Draft object is created from a set of faces, then all replaced material acts as one object. Therefore, operations such as deleting and suppressing, for example, affect all faces that comprise the Draft object.
See Also

Draft Members