Solid Edge Part Type Library
DividedParts Collection
Members 
Description
Represents a collection of a DividedPart objects.
Remarks
When the first item is added to the DividedParts collection, a second member is automatically added, as the nature of dividing parts is such that there must be two or more pieces. It is not necessary to populate the last piece, but it always exists in the collection. Its Order is automatically maintained by the system. Before calling Populate on the last member, you must provide a value for its DocumentName.
See Also

DividedParts Members