Solid Edge Part Type Library
ShowDimensions Property
Description
Controls the display of dimensions for the feature object.
Property type
Read-write property
Syntax
Visual Basic
Public Property ShowDimensions As Boolean
Remarks
If this property is True, the dimensions are displayed; if False, the dimensions are hidden.
See Also

ChangeBendAngle Object  | ChangeBendAngle Members  | Solid Edge V17 - What's New