Solid Edge Part Type Library
Chamfer Object
Members 
Description
An occurrence of a Chamfer object.
Object Model
Chamfer ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionFaceStyle ObjectSuppressVariable ObjectApplication Object
Remarks
The Chamfer object defines a chamfer feature along the edge of a solid. The orientation of the chamfer relative to the faces can be at a specified angle and distance from the common edge, or it can be defined as two specified distances from the common edge. A Chamfer object cannot exist alone; it can only be material removed at the common edge of two faces of an existing part.
See Also

Chamfer Members