AccuracyFactor | Set or Get accuracy factor of blank. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
HardeningCoefficient | Set or Get hardening coefficient of blank . |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
offsetDistance | Set or Get offset value for blank. |
Parent | Returns the parent object for the referenced object. |
RemoveLoopsOption | Set or Get remove loops setting of blank. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
StrengthCoefficient | Set or Get strength coefficient value of blank. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | |
Thickness | Set or Get thickness value of blank. |
Type | Specifies the type of the object being referenced. |