Solid Edge Part Type Library
RemoveLoopsOption Property
Collapse All
Expand All
Solid Edge Part Type Library
>
BlankSurface Object
: RemoveLoopsOption Property
Description
Get or Set remove loops option for blank surface.
Property type
Read-write property
Syntax
Visual Basic
Public Property RemoveLoopsOption As Boolean
Remarks
If ‘true’, this option will remove interior loops of the input faces selected.
See Also
BlankSurface Object
|
BlankSurface Members