Solid Edge Framework Type Library
AddToLocateFilter Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
DISEMouse Object
: AddToLocateFilter Method
Valid values are members of the seLocateFilterConstants constant set.
Description
Specifies what types of objects the Mouse can locate.
Syntax
Visual Basic
Public Sub AddToLocateFilter( _ ByVal
lFilter
As Long _ )
Parameters
lFilter
Valid values are members of the seLocateFilterConstants constant set.
See Also
DISEMouse Object
|
DISEMouse Members