Solid Edge Framework Type Library : DISEMouse Object |
AddToLocateFilter | Specifies what types of objects the Mouse can locate. |
ClearLocateFilter | Clears the locate filter for the referenced Mouse object. |
PointOnGraphic | Returns the actual point on the element returned from a locate operation. |
DynamicsMode | Sets and returns the dynamics mode for the referenced object. |
EnabledDrag | Sets and returns the enabling of drag events. |
EnabledMove | Sets and returns the enabling of move events for the referenced object. |
InterDocumentLocate | Specifies whether to locate keypoints or other objects in documents other than the active document. |
LastDownEventButton | Returns the last down event button. |
LastDownEventShift | Returns the last down event shift code. |
LastDownEventWindow | Returns the last down event window. |
LastDownEventX | Returns the last mouse down event x position. |
LastDownEventY | Returns the last mouse down event y position. |
LastDownEventZ | Returns the last mouse down event z position. |
LastEventButton | Returns the last event button. |
LastEventShift | Returns the last event shift code. |
LastEventType | Returns the last event window's type. |
LastEventWindow | Returns the last event window for the referenced object. |
LastEventX | Returns the last mouse event x position. |
LastEventY | Returns the last mouse event y position. |
LastEventZ | Returns the last mouse event z position. |
LastMoveEventButton | Returns the last move event button. |
LastMoveEventShift | Returns the last move event shift code. |
LastMoveEventWindow | Returns the last move event window. |
LastMoveEventX | Returns the last mouse move event x position. |
LastMoveEventY | Returns the last mouse move event y position. |
LastMoveEventZ | Returns the last mouse move event z position. |
LastUpEventButton | Returns the last up event button. |
LastUpEventShift | Returns the last up event shift code. |
LastUpEventWindow | Returns the last up event window. |
LastUpEventX | Returns the last mouse up event x position. |
LastUpEventY | Returns the last mouse up event y position. |
LastUpEventZ | Returns the last mouse up event z position. |
LocateFrontToBack | Specifies whether to locate front to back. |
LocateMode | Sets and returns the locate mode for the referenced object. |
PauseLocate | Sets and returns the paused locate value. |
ScaleMode | Sets and returns the scale mode. |
WindowTypes | Sets and returns the Window types. |