Solid Edge FrameworkSupport Type Library
BreakLineDirection Property
Description
Sets and returns the direction (left or right) in which the break line runs along the x axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property BreakLineDirection As Boolean
Remarks
If BreakLineDirection is True, the break line points to the right of the dimensioning object; if False, the break line points to the left. This property is only enabled if the BreakLine property is True.
See Also

WeldSymbol Object  | WeldSymbol Members